rpos::features::motion_planner::Path Class
A Path Object is a collection container of rpos::core::Location objects.
Header File
rpos/features/motion_planner.h
Applies to
- Slamware
Constructors
/**
* Construct a path object with a set of points.
*/
Path(const std::vector<core::Location>& points);
please refer to core::Location.
/**
* Copy Constructor.
*/
Path(const Path&);
Operators
/**
* Assignment operator.
*/
Path& operator=(const Path&);
Methods
/**
* Get all the points of the path.
*/
std::vector<rpos::core::Location>& getPoints();
For details, please refer to rpos::core::Location.
/**
* Truncate the path with points exceed the size limit to be removed.
*/
rpos::features::motion_planner::Path truncate(unsigned int size);