rpos::features::MotionPlanner Class
Provides all kinds of navigation functions, including dynamic path finding, autonomous obstacle avoidance, auto docking and more.
Header File
rpos/features/motion_planner.h
Applies to
- Slamware
Parent Class
Methods
/**
* Go back to home dock
*/
actions::MoveAction goHome(const rpos::features::motion_planner::GoHomeOptions& options);
| Parameter | Type | Description |
|---|---|---|
| options | const features::motion_planner::GoHomeOptions& |
options of GohomeAction |
| return | actions::MoveAction |
action object |
/**
* Go back to home dock with default options, it's compatible with 2.x firmware
*/
actions::MoveAction goHome();
/**
* Requires the robot to move to a set of key points (milestone) specified by the parameters.
* The robot will try its best to reach each points specified. In case of obstacles occurs, the robot will avoid hitting them by planning a valid path.
*/
rpos::actions::MoveAction moveTo(
const std::vector<rpos::core::Location>& locations,
bool appending
);
| Parameter | Type | Description |
|---|---|---|
| locations | const std::vector<rpos::core::Location>& |
Points collection that the robot should reach |
| appending | bool | Once set to true, a current working action (if any) won't get aborted and the key points specified by the function will be pending to the task queue. |
/**
* Requires the robot to move to a key point (milestone) specified by the parameters.
* The robot will try its best to reach the point specified. In case of obstacles occurs, the robot will avoid hitting them by planning a valid path.
*/
rpos::actions::MoveAction moveTo(
const rpos::core::Location& location,
bool appending
);
| Parameter | Type | Description |
|---|---|---|
| location | const std::vector<rpos::core::Location>& |
Point that the robot should reach |
| appending | bool | Once set to true, a current working action (if any) won't get aborted and the key points specified by the function will be pending to the task queue. |
/**
* Requires the robot to move to a set of key points (milestone) specified by the parameters and turn to a specified heading.
* The robot will try its best to reach each points specified. In case of obstacles occurs, the robot will avoid hitting them by planning a valid path.
*/
rpos::actions::MoveAction moveTo(
const std::vector<rpos::core::Location>& locations,
const motion_planner::MoveOptions& options
);
| Parameter | Type | Description |
|---|---|---|
| locations | const std::vector<rpos::core::Location>& |
Points collection that the robot should reach |
| options | const motion_planner::MoveOptions& |
Motion Options |
/**
* Requires the robot to move to a key point (milestone) specified by the parameters and turn to a specified heading in the end of the action.
* The robot will try its best to reach the point specified. In case of obstacles occurs, the robot will avoid hitting them by planning a valid path.
*/
rpos::actions::MoveAction moveTo(
const rpos::core::Location& location,
const motion_planner::MoveOptions& options
);
| Parameter | Type | Description |
|---|---|---|
| location | const std::vector<rpos::core::Location>& |
Point that the robot should reach |
| options | const motion_planner::MoveOptions& |
Motion Options |
/**
* Make the robot move along with the specified direction. No obstle avoidance or path planning will be performed.
*/
rpos::actions::MoveAction moveBy(const rpos::core::Direction& direction);
For details, please refer to
rpos::core::Direction.
/**
* Make the robot move along with the specified direction.
*/
rpos::actions::MoveAction moveBy(
const rpos::core::Direction& direction,
const motion_planner::MoveOptions& options
);
For details, please refer to
rpos::core::Directionandmotion_planner::MoveOptions.
/**
* Make the robot move with a turning angle.
*/
rpos::actions::MoveAction moveBy(
float theta,
const motion_planner::MoveOptions& options
);
For details, please refer to
motion_planner::MoveOptions.
/**
* Make the robot turn to the specified heading.
*/
rpos::actions::MoveAction rotateTo(const rpos::core::Rotation& orientation);
For details, please refer to
rpos::core::Rotation.
/**
* Make the robot turn to the specified heading.
*/
rpos::actions::MoveAction rotateTo(
const rpos::core::Rotation& orientation,
const motion_planner::MoveOptions& options
);
For details, please refer to
rpos::core::Rotationandmotion_planner::MoveOptions.
/**
* Make the robot turn by the specified angle.
*/
rpos::actions::MoveAction rotate(const rpos::core::Rotation& rotation);
For details, please refer to
rpos::actions::MoveActionandrpos::core::Rotation.
/**
* Make the robot turn by the specified angle.
*/
rpos::actions::MoveAction rotate(
const rpos::core::Rotation& rotation,
const motion_planner::MoveOptions& options
);
For details, please refer to
rpos::core::Rotationandmotion_planner::MoveOptions.
/**
* Require the robot to perform self relocalization to recover it post on the map. The robot will move.
*/
rpos::actions::MoveAction recoverLocalization(
const core::RectangleF& area,
const motion_planner::RecoverLocalizationOptions& options
);
For details, please refer to
rpos::actions::MoveAction,core::RectangleFandmotion_planner::RecoverLocalizationOptions.
/**
* Require bypass the navigation system and direct control the robot motion. The detailed walking speed and turning speed can be set via the returned ```VelocityControlMoveAction``` action.
*/
rpos::actions::VelocityControlMoveAction velocityControl();
For details, please refer to rpos::actions::VelocityControlMoveAction.
/**
* Retrieve the current action of the robot. If the Action::isEmpty() of the returned object is false, there is no action working at all.
*/
rpos::actions::MoveAction getCurrentAction();
For details, please refer to rpos::actions::MoveAction.
/**
* Require the SLAMWARE system to find a path to the destination specified by the parameter. The path found will be returned.
*/
rpos::features::motion_planner::Path searchPath(const rpos::core::Location&);
For details, please refer to rpos::features::motion_planner::Path and rpos::core::Location.
/**
* get all supported motion strategies.
* motion strategy contains a series of configuration items that affect machine behavior.
*/
std::vector<std::string> enumSupportedMotionStrategies();
/**
* set a motion strategy to robot
*/
bool setMotionStrategy(const std::string& strategy);
/**
* get current motion strategy
*/
std::string getCurrentMotionStrategy();