rpos::features::system_resource::LaserScan Class
LaserScan is the collection of a series of LaserPoint objects that represents a scan iteration of an LIDAR sensor.
Header File
rpos/features/system_resource.h
Applies to
- Slamware
- Mapper
Constructors
/**
*Construct a new Object based on a set of rpos::core::LaserPoint.
*/
LaserScan(const std::vector<rpos::core::LaserPoint>&);
/**
* Copy contructors.
*/
LaserScan(const LaserScan&);
Operators
/**
* Assignment operator.
*/
LaserScan& operator=(const LaserScan&);
Methods
/**
* Retrieves the LaserPoint data collection.
*/
const std::vector<core::LaserPoint>& getLaserPoints() const;
/**
* Set the scan points data to the object.
*/
void setLaserPoints(const std::vector<core::LaserPoint>& data, rpos::system::types::_u64 timestamp);
| Paramer Name | Type | Description |
|---|---|---|
| data | const std::vector<core::LaserPoint>& |
The LaserPoint collection data to be set |
| timestamp | rpos::system::types::_u64 |
Timestamp of the laser scan |
/**
* Set the centor pose of the current laser scan.
*/
void setLaserPointsPose(const rpos::core::Pose& pose);
/**
* Retrieve the centor pose of the current laser scan.
*/
const rpos::core::Pose& getLaserPointsPose() const;
/**
* Set wheter the current scan object contains valid pose data.
*/
void setHasPose(bool hasPose);
/**
* Returns wheter the current scan object contains valid pose data.
*/
bool getHasPose() const;