rpos::features::location_provider::Map Class
Base class of Map.
Header File
rpos/features/location_provider/map.h
Applies to
- Slamware
- Mapper
Methods
/**
* Retrieves the area of the current map.
*/
rpos::core::RectangleF& getMapArea() const;
For details, please refer to rpos::core::RectangleF.
/**
* Retrieves the the upper-left point poistion of the map data.
*/
rpos::core::Vector2f& getMapPosition() const;
For details, please refer to rpos::core::Vector2f.
/**
* Retrieves the pixel size (in X,Y dimensions) of the map.
*/
rpos::core::Vector2i& getMapDimension() const;
For details, please refer to rpos::core::Vector2i.
/**
* Retrieves the real world size of each cell (or pixel) of the map. In meter units.
*/
rpos::core::Vector2f& getMapResolution() const;
/**
* Retrieve the map updated timestamp.
*/
rpos::system::types::timestamp_t getMapTimestamp();
/**
* Retrieve the map data in raw byte stream.
*/
std::vector<_u8>& getMapData() const;
/**
* Retrieves the map type.
*/
MapType getMapType() const;
| Return Value | Description | Related Class |
|---|---|---|
MapTypeBitmap8Bit |
The map is a grid map with each pixel is a 8bit cell | rpos::features::location_provider::BitmapMap |
MapTypePointmap |
Point map | rpos::features::location_provider::PointsMap |
/**
* Read map data from the specified input stream.
*/
virtual bool readFromStream(rpos::system::io::IStream &in);
/**
* Write the map data from the specified output stream.
*/
virtual bool writeToStream(rpos::system::io::IStream &out) const;
/**
* Case the map object to its subclass type.
*/
template<class MapT> MapT cast();