rpos::core::ImuBitMap Enum Type

ImuBitMap Defines all the available part of Imu data

Header File

rpos/core/pose.h

Enum Items

Item Description
NO_IMU_READY No data is available in the related imu.
QUATERNION_READY Quaternion is available in the related imu.
CALIBRATED_ACC_READY Calibrated acc is available in the related imu.
CALIBRATED_GYRO_READY Calibrated gryro is available in the related imu.
CALIBRATED_COMPASS_READY Calibrated compass is available in the related imu.
RAW_ACC_READY Raw acc is available in the related imu.
RAW_GYRO_READY Raw gyro is available in the related imu.
RAW_COMPASS_READY Raw compass is available in the related imu.
FUSION_6DOF_READY Fuse dimension of the imu data.
FUSION_9DOF_READY Fuse dimension of the imu data.