rpos::features::artifact_provider::ArtifactUsage Enum Type
ArtifactUsage contains all available artifact usage type.
Header Files
rpos/features/artifact_provider/feature.h
Applies to
- Slamware
Enums
| Type | Value | Description |
|---|---|---|
ArtifactUsageVirtualWall |
0 | Virtual walls works just like walls, they blocks robot move through |
ArtifactUsageVirtualTrack |
1 | Virtual tracks are used to guide robot's movement. Robot will try its best to move along with virtual tracks |
ArtifactUsageScheduleArea |
2 | Schedule areas are used to achieve multi-robot collaborative behavior |
ArtifactUsageMaintenanceArea |
3 | Maintenance area has mutable environment, slamware will automatically update map of this area |
ArtifactUsageForbiddenArea |
4 | Forbidden area means robot should not enter this area, but if accidentally entered, it can escape |