rpos::features::system_resource::DeviceInfo Class
Interface helps to retrieve device information.
Header File
rpos/features/system_resource/device_info.h
Applies to
- Slamware
- Mapper
Constructor
DeviceInfo()
default constructor
DeviceInfo(const DeviceInfo&)
copy constructor
Operators
DeviceInfo& operator=(const DeviceInfo&)
Assignment operator
Methods
std::string deviceID() const
Retrieves the device ID string of the SLAMWARE System
std::string& deviceID()
Retrives the device ID string of the SLAMWARE System
int manufacturerID() const
Retrieves the manufacturer ID of the robot base
int& manufacturerID()
Retrieves the manufacturer ID of the robot base
std::string manufacturerName() const
Retrieves the manufacture name of the robot base
std::string& manufacturerName()
Retrieves the manufacture name of the robot base
int modelID() const
Retrieves the model ID of the robot base
int& modelID()
Retrieves the model ID of the robot base
std::string modelName() const
Retrieves the model name of the robot base
std::string& modelName()
Retrieves the model name of the robot base
std::string hardwareVersion() const
Retrieves the hardware version string of the SLAMWARE System
std::string& hardwareVersion()
Retrieves the hardware version string of the SLAMWARE System
std::string softwareVersion() const
Retrieves the software version string of the SLAMWARE System
std::string& softwareVersion()
Retrieves the software version string of the SLAMWARE System