The tracking info structure. More...
#include <aurora_pubsdk_objects.h>
Public Attributes | |
| uint64_t | timestamp_ns |
| The timestamp of the tracking. More... | |
| slamtec_aurora_sdk_image_desc_t | left_image_desc |
| The description of the left image. More... | |
| slamtec_aurora_sdk_image_desc_t | right_image_desc |
| The description of the right image. More... | |
| uint32_t | is_stereo |
| Whether the tracking is stereo. | |
| uint32_t | tracking_status |
| The tracking status value. More... | |
| slamtec_aurora_sdk_pose_se3_t | pose |
| The pose of the tracking (base to world) More... | |
| uint32_t | keypoints_left_count |
| The count of the keypoints of the left image. More... | |
| uint32_t | keypoints_right_count |
| The count of the keypoints of the right image. More... | |
The tracking info structure.
The tracking info structure contains the tracking information.
NOTICE: the image provided by tracking info has been lossy compressed during transmission
to retrieve the original image, please use the raw image data callback
The raw image subscription must be enabled first
| uint32_t _slamtec_aurora_sdk_tracking_info::keypoints_left_count |
The count of the keypoints of the left image.
The count of the keypoints of the left image is the count of the keypoints of the left image.
| uint32_t _slamtec_aurora_sdk_tracking_info::keypoints_right_count |
The count of the keypoints of the right image.
The count of the keypoints of the right image is the count of the keypoints of the right image.
| slamtec_aurora_sdk_image_desc_t _slamtec_aurora_sdk_tracking_info::left_image_desc |
The description of the left image.
The description of the left image is the description of the left image.
| slamtec_aurora_sdk_pose_se3_t _slamtec_aurora_sdk_tracking_info::pose |
The pose of the tracking (base to world)
The pose of the tracking is the pose of the tracking.
| slamtec_aurora_sdk_image_desc_t _slamtec_aurora_sdk_tracking_info::right_image_desc |
The description of the right image.
The description of the right image is the description of the right image.
| uint64_t _slamtec_aurora_sdk_tracking_info::timestamp_ns |
The timestamp of the tracking.
The nanoseconds timestamp of the tracking frame
| uint32_t _slamtec_aurora_sdk_tracking_info::tracking_status |
The tracking status value.
The tracking status value is the value of the slamtec_aurora_sdk_tracking_status_t