The session config structure. More...
#include <aurora_pubsdk_objects.h>
Public Attributes | |
| uint32_t | version |
| The session config version. More... | |
| uint32_t | reserved |
| The reserved field. More... | |
The session config structure.
The session config structure contains the session configuration.
| uint32_t _slamtec_aurora_sdk_session_config_t::reserved |
The reserved field.
The reserved field must be 0.
| uint32_t _slamtec_aurora_sdk_session_config_t::version |
The session config version.
The session config version is the version of the session config. Set to 0 for now.