The map description structure. More...
#include <aurora_pubsdk_objects.h>
Public Attributes | |
| uint32_t | map_id |
| The ID of the map. | |
| uint32_t | map_flags |
| The flags of the map, check enum slamtec_aurora_sdk_map_flags_t for more details. | |
| uint64_t | keyframe_count |
| The count of the keyframes in the map. | |
| uint64_t | map_point_count |
| The count of the map points in the map. | |
| uint64_t | keyframe_id_start |
| The ID of the first keyframe in the map. | |
| uint64_t | keyframe_id_end |
| The ID of the last keyframe in the map. | |
| uint64_t | map_point_id_start |
| The ID of the first map point in the map. | |
| uint64_t | map_point_id_end |
| The ID of the last map point in the map. | |
The map description structure.
The map description structure contains the map description.