The image description structure. More...
#include <aurora_pubsdk_objects.h>
Public Attributes | |
| uint32_t | width |
| The width of the image. More... | |
| uint32_t | height |
| The height of the image. More... | |
| uint32_t | stride |
| The stride of the image. More... | |
| uint32_t | format |
| The format of the image. More... | |
| uint32_t | data_size |
| The size of the image data in bytes. More... | |
The image description structure.
The image description structure contains the description of an image.
| uint32_t _slamtec_aurora_sdk_image_desc_t::data_size |
The size of the image data in bytes.
The size of the image data is the size of the image data in bytes.
| uint32_t _slamtec_aurora_sdk_image_desc_t::format |
The format of the image.
The format of the image is the format of the image.
0: gray, 1: rgb, 2: rgba
| uint32_t _slamtec_aurora_sdk_image_desc_t::height |
The height of the image.
The height of the image is the height of the image.
| uint32_t _slamtec_aurora_sdk_image_desc_t::stride |
The stride of the image.
The stride of the image is the stride of the image.
| uint32_t _slamtec_aurora_sdk_image_desc_t::width |
The width of the image.
The width of the image is the width of the image.