SLAMTEC Aurora Public Remote SDK  1.2.0-rtm
_slamtec_aurora_sdk_device_status_desc Struct Reference

The device status structure. More...

#include <aurora_pubsdk_objects.h>

Public Attributes

slamtec_aurora_sdk_device_status_t status
 
uint64_t timestamp_ns
 

Detailed Description

The device status structure.

The device status structure contains the status of the device.


The documentation for this struct was generated from the following file: